What is difference between Validation and Target validation in eIQ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is difference between Validation and Target validation in eIQ?

2,545 次查看
nnxxpp
Contributor IV

My question is same as the title.

As my understanding Validation is for local host and Target validation  is the board. Is that right? 

If Target validation  is the board it means that we need to connect board to PC and eIQ will copy all script for evaluation to the board. After evaluation eIQ will remove data from the board. Is that right?

I have one more question. Does eIQ have feature that allow us to measure inference time on the board (emulation)?

标签 (1)
0 项奖励
回复
3 回复数

2,493 次查看
nnxxpp
Contributor IV

Hi @Harry_Zhang 

By clicking the VALIDATION TARGET button, a modal window appears to insert new
target devices or select an existing device to perform the validation on. You can also choose to not select a
target and validate the model on your local host (your computer) by default.
Clicking the “VALIDATE” button starts the validation process.

You can refer to the eIQ Toolkit User Guide.

eIQ_Toolkit_v1.13.1\docs\eIQ_Toolkit_UG.pdf

BR

Harry

I will check it now. Thank you.

0 项奖励
回复

2,497 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @nnxxpp 

By clicking the VALIDATION TARGET button, a modal window appears to insert new
target devices or select an existing device to perform the validation on. You can also choose to not select a
target and validate the model on your local host (your computer) by default.
Clicking the “VALIDATE” button starts the validation process.

You can refer to the eIQ Toolkit User Guide.

eIQ_Toolkit_v1.13.1\docs\eIQ_Toolkit_UG.pdf

BR

Harry

0 项奖励
回复

2,486 次查看
nnxxpp
Contributor IV

@Harry_Zhang 

I connect my old board MIMXRT via debugging USB. I don't see anything in the remote device window. You can see in the image . What I need to do next?

0 项奖励
回复