Unable to open probe index 1/Unable to update firmware - FRDM MCXN947

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to open probe index 1/Unable to update firmware - FRDM MCXN947

973 次查看
DanielCCMx
Contributor I

Hello, I cannot update the firmware on my FRDM MCXN947, I get below errors

DanielCCMx_0-1733860435527.pngDanielCCMx_1-1733860441230.png

After that when i tried to debug i get the error "Unable to open probe index 1. Error Probe not open"

DanielCCMx_2-1733860601114.png

DanielCCMx_3-1733860662947.png

DanielCCMx_4-1733860676260.png

DanielCCMx_5-1733860690457.png

 

( 5) Remote configuration complete

Reconnected to existing LinkServer process.

Connecting to probe 1 core 0 (using server started externally) reports:

'Ee(42). Could not connect to core.'

Retrying...

Reconnected to existing LinkServer process.

Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.

Failed on connect: Ee(42). Could not connect to core.

No connection to chip's debug port

 

 

The wire and connection is good, the device is even detected in device manager, but somehow this is not working

DanielCCMx_6-1733860806210.png

 

I already uninstall and install everything

Could someone help me pls?

 

 

 

标签 (1)
0 项奖励
回复
3 回复数

948 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that you connect the J17 Type C USB connector to PC via USB cable to download and debug. In the case, for all the jumper, you only need to close J22 and J24 two jumper, open all the other jumper.

I attach the picture, pls check if the jumper is correct or not.

xiangjun_rong_0-1733885508921.png

 

If you still have issue after you configure the jumper, pls update the ticket.

Hope it can help you

BR

XiangJun Rong

 

 

0 项奖励
回复

929 次查看
DanielCCMx
Contributor I

Hello @xiangjun_rong 

Yes, USB Type C is connected to J17 and the only two closed jumpers are J22 and J24, all the other jumpers are opened. 

I was able to update the firmware by following the steps mentioned in https://community.nxp.com/t5/MCUXpresso-IDE/FRDM-MCXN947/m-p/1816631 

Nevertheless that didn't solve my issue, i still face the error "Unable to open probe index 1" when i try to debug. 

I can see that the probe is detected by running this command, but it is not opened yet. 

DanielCCMx_0-1733930072485.png

 

 

0 项奖励
回复

912 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

This is a trick, but I do not guarantee it can solve your issue, anyway, pls have a try.

On the FRDM-MCXN947 board, holding the ISP SW3 button, then insert the J17 USB connector to power up the board, then release the ISP SW3.

The first step is clicking "Build", the second step is  clicking "Debug"

xiangjun_rong_0-1733973920520.png

 

Hope it is helpful.

BR

XiangJun Rong

 

0 项奖励
回复