Could I use the CodeWarrior (CW_MCU_v11.1_b181224_PE.exe) to download the pgm file to the MCF54415 M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Could I use the CodeWarrior (CW_MCU_v11.1_b181224_PE.exe) to download the pgm file to the MCF54415 M

2,046件の閲覧回数
andylong_2024
Contributor III

1. Could I use the CodeWarrior (CW_MCU_v11.1_b181224_PE.exe) to download the pgm file to the MCF54415 MCU using BDM tools?
2. And is a license necessary during the downloading of the pgm file?
thanks

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,502件の閲覧回数
andylong_2024
Contributor III

ok. thanks

0 件の賞賛
返信

1,598件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I don't think CodeWarrior for MCU V11.1 IDE software could support to program PGM(portable gray map) file via BDM debugger tool.

The general image format CodeWarrior supported are S19, bin and elf.

Mike

0 件の賞賛
返信