Ubuntu EIQ Tookit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ubuntu EIQ Tookit

2,187 Views
Sherlock987
Contributor I

Hello, I have downloaded the EIQ Toolkit with ubuntu 20.04, unzipped it and ran the *.bin program. But when i try to run the program, it crashes with the following error:

/opt/nxp/eIQ_Toolkit_v1.12.1/bin/eiqenv.sh

/opt/nxp/eIQ_Toolkit_v1.12.1/eiq-portal

 

Unhandled Promise Rejection
TypeError: Cannot read property 'kill' of null
at /opt/nxp/eIQ_Toolkit_v1.12.1/resources/app.asar/background.js:2:564394

Labels (1)
0 Kudos
Reply
3 Replies

2,057 Views
Sherlock987
Contributor I

Sorry, I was using the Ubuntu version 22.04 and did not notice that the tool is supported for 20.04. I installed virtualbox for workaround

0 Kudos
Reply

2,037 Views
Joey_z
NXP Employee
NXP Employee

hi,Sherlock987

I'm glad your problem is solved. 

BR

Xu Zhang

0 Kudos
Reply

2,110 Views
Joey_z
NXP Employee
NXP Employee

hi,Sherlock987

I have received your case and I'm processing it, I'll provide feedback soon. Thank you for your patience in advance.

 

BR

Xu Zhang

0 Kudos
Reply