Ubuntu EIQ Tookit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ubuntu EIQ Tookit

2,254件の閲覧回数
Sherlock987
Contributor I

Hello, I have downloaded the EIQ Toolkit with ubuntu 20.04, unzipped it and ran the *.bin program. But when i try to run the program, it crashes with the following error:

/opt/nxp/eIQ_Toolkit_v1.12.1/bin/eiqenv.sh

/opt/nxp/eIQ_Toolkit_v1.12.1/eiq-portal

 

Unhandled Promise Rejection
TypeError: Cannot read property 'kill' of null
at /opt/nxp/eIQ_Toolkit_v1.12.1/resources/app.asar/background.js:2:564394

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,124件の閲覧回数
Sherlock987
Contributor I

Sorry, I was using the Ubuntu version 22.04 and did not notice that the tool is supported for 20.04. I installed virtualbox for workaround

0 件の賞賛
返信

2,104件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,Sherlock987

I'm glad your problem is solved. 

BR

Xu Zhang

0 件の賞賛
返信

2,177件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,Sherlock987

I have received your case and I'm processing it, I'll provide feedback soon. Thank you for your patience in advance.

 

BR

Xu Zhang

0 件の賞賛
返信