UART Setup on FRDM-MCXN947

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART Setup on FRDM-MCXN947

Jump to solution
2,431 Views
John_Adams
Contributor I

Hello,
I'm trying to reset LPUART to the frequency from FRO_HF (48 MHz) and keep baudrate 230400. Unfortunately I can't get it to work despite setting the CLK for the UART and baudrate. Have I forgotten something? Can I somehow change the divider?

 

    /* attach FRO HS to FLEXCOMM7 */
    CLOCK_SetClkDiv(kCLOCK_DivFlexcom7Clk, 1u);
    CLOCK_AttachClk(kFRO_HF_DIV_to_FLEXCOMM7);

 

My LPUART setup:

 

    LPUART_GetDefaultConfig(&config);
    config.baudRate_Bps = 230400;
    config.isMsb        = false;
    config.enableTx     = false;
    config.enableRx     = true;

    PRINTF("Frequency: %d\r\n", CLOCK_GetLPFlexCommClkFreq(7u));
    freq = CLOCK_GetLPFlexCommClkFreq(7u);
    LPUART_Init(LPUART7, &config, freq);
    uint32_t divider = ((LPUART7->BAUD & LPUART_BAUD_SBR_MASK) >> LPUART_BAUD_SBR_SHIFT);

    DisableIRQ(LPUART7_IRQn);
    /* Enable RX interrupt. */
    LPUART_EnableInterrupts(LPUART7, kLPUART_TransmissionCompleteInterruptEnable);
    EnableIRQ(LPUART7_IRQn);

 

 

 

Thank you

John Adams

 

Labels (3)
0 Kudos
Reply
1 Solution
2,151 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @John_Adams,

Of course, that would be any of the other LPUART examples that we provide in our SDK:

EdwinHz_0-1733516758588.png

 

BR,
Edwin.

 

View solution in original post

0 Kudos
Reply
7 Replies
2,409 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @John_Adams,

Please make sure you are also initializing the appropriate pins on the pin_mux.c file under board folder.

BR,
Edwin.

0 Kudos
Reply
2,379 Views
John_Adams
Contributor I

Thank you for your answer @EdwinHz 
I have the pins installed, I don't have a problem that LPUART doesn't work at all, I have a problem that UART doesn't keep up with the speed of communication on FRO_12M. I am trying to increase the frequency, but I have the feeling that the baudrate is not set correctly, how can I change the divider?

John Adams

0 Kudos
Reply
2,328 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @John_Adams,

You can chance the FC7 divider by using the line you previously mentioned:

CLOCK_SetClkDiv(kCLOCK_DivFlexcom7Clk, 1u);

 However, this is already at the lowest division possible. increasing the divider will only decrease the frequency. If you wish to increase the FC7 frequency, you can try changing the source clock to another source, like the PLL divided clock (pll_clk_div) using:

CLOCK_AttachClk(kPLL_DIV_to_FLEXCOMM7);

Just make sure you are enabling this PLL divided clock by using:

CLOCK_AttachClk(kPLL0_to_PLLCLKDIV);
CLOCK_SetClkDiv(kCLOCK_DivPllClk, 1U);

BR,
Edwin.

0 Kudos
Reply
2,221 Views
John_Adams
Contributor I
Thank you,
Also I will have to use LPUART FIFO, can you please advise me how to read sequentially the data from this FIFO queue?

John Adams
0 Kudos
Reply
2,208 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @John_Adams,

You could sequentially read the FIFO queue by letting the eDMA automatically handle these reads. Please look at the "lpuart_edma_transfer" example code, as it shows how the eDMA handles the FIFO reads automatically.

BR,
Edwin.

0 Kudos
Reply
2,179 Views
John_Adams
Contributor I
Thank you Edwin,
I will look at the example. Just by chance, is there any example that would use FIFO and not use EDMA?

John Adams

0 Kudos
Reply
2,152 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @John_Adams,

Of course, that would be any of the other LPUART examples that we provide in our SDK:

EdwinHz_0-1733516758588.png

 

BR,
Edwin.

 

0 Kudos
Reply