UART Setup on FRDM-MCXN947

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

UART Setup on FRDM-MCXN947

跳至解决方案
2,424 次查看
John_Adams
Contributor I

Hello,
I'm trying to reset LPUART to the frequency from FRO_HF (48 MHz) and keep baudrate 230400. Unfortunately I can't get it to work despite setting the CLK for the UART and baudrate. Have I forgotten something? Can I somehow change the divider?

 

    /* attach FRO HS to FLEXCOMM7 */
    CLOCK_SetClkDiv(kCLOCK_DivFlexcom7Clk, 1u);
    CLOCK_AttachClk(kFRO_HF_DIV_to_FLEXCOMM7);

 

My LPUART setup:

 

    LPUART_GetDefaultConfig(&config);
    config.baudRate_Bps = 230400;
    config.isMsb        = false;
    config.enableTx     = false;
    config.enableRx     = true;

    PRINTF("Frequency: %d\r\n", CLOCK_GetLPFlexCommClkFreq(7u));
    freq = CLOCK_GetLPFlexCommClkFreq(7u);
    LPUART_Init(LPUART7, &config, freq);
    uint32_t divider = ((LPUART7->BAUD & LPUART_BAUD_SBR_MASK) >> LPUART_BAUD_SBR_SHIFT);

    DisableIRQ(LPUART7_IRQn);
    /* Enable RX interrupt. */
    LPUART_EnableInterrupts(LPUART7, kLPUART_TransmissionCompleteInterruptEnable);
    EnableIRQ(LPUART7_IRQn);

 

 

 

Thank you

John Adams

 

标签 (3)
0 项奖励
回复
1 解答
2,144 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @John_Adams,

Of course, that would be any of the other LPUART examples that we provide in our SDK:

EdwinHz_0-1733516758588.png

 

BR,
Edwin.

 

在原帖中查看解决方案

0 项奖励
回复
7 回复数
2,402 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @John_Adams,

Please make sure you are also initializing the appropriate pins on the pin_mux.c file under board folder.

BR,
Edwin.

0 项奖励
回复
2,372 次查看
John_Adams
Contributor I

Thank you for your answer @EdwinHz 
I have the pins installed, I don't have a problem that LPUART doesn't work at all, I have a problem that UART doesn't keep up with the speed of communication on FRO_12M. I am trying to increase the frequency, but I have the feeling that the baudrate is not set correctly, how can I change the divider?

John Adams

0 项奖励
回复
2,321 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @John_Adams,

You can chance the FC7 divider by using the line you previously mentioned:

CLOCK_SetClkDiv(kCLOCK_DivFlexcom7Clk, 1u);

 However, this is already at the lowest division possible. increasing the divider will only decrease the frequency. If you wish to increase the FC7 frequency, you can try changing the source clock to another source, like the PLL divided clock (pll_clk_div) using:

CLOCK_AttachClk(kPLL_DIV_to_FLEXCOMM7);

Just make sure you are enabling this PLL divided clock by using:

CLOCK_AttachClk(kPLL0_to_PLLCLKDIV);
CLOCK_SetClkDiv(kCLOCK_DivPllClk, 1U);

BR,
Edwin.

0 项奖励
回复
2,214 次查看
John_Adams
Contributor I
Thank you,
Also I will have to use LPUART FIFO, can you please advise me how to read sequentially the data from this FIFO queue?

John Adams
0 项奖励
回复
2,201 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @John_Adams,

You could sequentially read the FIFO queue by letting the eDMA automatically handle these reads. Please look at the "lpuart_edma_transfer" example code, as it shows how the eDMA handles the FIFO reads automatically.

BR,
Edwin.

0 项奖励
回复
2,172 次查看
John_Adams
Contributor I
Thank you Edwin,
I will look at the example. Just by chance, is there any example that would use FIFO and not use EDMA?

John Adams

0 项奖励
回复
2,145 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @John_Adams,

Of course, that would be any of the other LPUART examples that we provide in our SDK:

EdwinHz_0-1733516758588.png

 

BR,
Edwin.

 

0 项奖励
回复