Temporarily disable reset pin on MCXC244

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Temporarily disable reset pin on MCXC244

841 Views
redwolf
Contributor I

Hello,

I am working with the MCXC244 microcontroller and would like to temporarily disable the reset function on the default reset pin (PTA20/RESET_b). I also want to have the ability to enable the reset function again when needed. Is there a way to achieve this?

Labels (1)
0 Kudos
Reply
3 Replies

789 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

By default, this pin will always be reset function unless the pin functionality is changed on the booted application. During boot process/power up it will stay at the default state.

Best regards,
Omar

0 Kudos
Reply

768 Views
redwolf
Contributor I
Hi Omar,
This is exactly what I’m aiming to do, modify the pin functionality in the booted application. I’ve disabled the RCM:RESET function in the pin configurator and configured the pin as a GPIO, but it still behaves like a reset pin.
0 Kudos
Reply

657 Views
ZhangJennie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply