Temporarily disable reset pin on MCXC244

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Temporarily disable reset pin on MCXC244

838 次查看
redwolf
Contributor I

Hello,

I am working with the MCXC244 microcontroller and would like to temporarily disable the reset function on the default reset pin (PTA20/RESET_b). I also want to have the ability to enable the reset function again when needed. Is there a way to achieve this?

标签 (1)
0 项奖励
回复
3 回复数

786 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

By default, this pin will always be reset function unless the pin functionality is changed on the booted application. During boot process/power up it will stay at the default state.

Best regards,
Omar

0 项奖励
回复

765 次查看
redwolf
Contributor I
Hi Omar,
This is exactly what I’m aiming to do, modify the pin functionality in the booted application. I’ve disabled the RCM:RESET function in the pin configurator and configured the pin as a GPIO, but it still behaves like a reset pin.
0 项奖励
回复

654 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport
0 项奖励
回复