SMBus support in MCX series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SMBus support in MCX series

802 Views
dav1
Contributor V

Hi,

 

Going through the more simple MCX'es, especially the MCXC series for an EC/SMC like application.

I can't seem to find any clear details on how/if SMBus is supported and what version?

SMBus 2.0 is probably bare minimum, but 3.0 with higher speeds (1MHz), and then 3.1 that some more recent battery-chargers make use of (for host notify) can be handy as battery-packs become more advanced.

 

Would be great with some info from the MCX product team

Labels (2)
Tags (2)
0 Kudos
Reply
3 Replies

423 Views
dav1
Contributor V

how about smbus support in the MCX A series? specifically: MCXA144VPJ

0 Kudos
Reply

774 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @dav1,

The MCX C series of MCUs does support SMBus, as mentioned on the "MCX C44X Sub-Family Reference Manual":

EdwinHz_0-1746550315448.png

However, as mentioned on the previous table, it supports version 2 of SMBus.

BR,
Edwin.

 

0 Kudos
Reply

796 Views
dav1
Contributor V

to give some context, here are a few recent and commonly used BMU's & chargers, all running SMBus 3.x

 

IC

Type

Manufacturer

SMBus Version

Features

ISL9241

Battery Charger

Renesas

3.0

NVDC, OTG, SMBus with PEC, telemetry

BQ24773

Battery Charger

Texas Instruments

3.0

Dynamic power, PEC, fast charge

BQ25720

Battery Charger

Texas Instruments

3.0

Wide input range, dual SMBus/I2C, PEC, dynamic power

MAX77960

Battery Charger

Analog Devices

3.0

Fast charging, PEC, power path control

BQ76952

Battery Monitor

Texas Instruments

3.1

Integrated balancing, PEC, high cell count support

ISL94216

Battery Monitor

Renesas

3.0

Group command, zone write, PEC

BQ40Z50-R2

Fuel Gauge

Texas Instruments

3.0

PEC, data flash, battery protection

BQ40Z80

Fuel Gauge

Texas Instruments

3.1

PEC, host notify, group command, data flash

BQ34Z100-G1

Fuel Gauge

Texas Instruments

3.0

PEC, host notify, battery management

MAX17330

Fuel Gauge

Analog Devices (Maxim)

3.0+

Group command, PEC, protection features

NCP81239

Power Delivery controller

ON Semiconductor

3.0

Telemetry, PEC, voltage regulation

LTC2977

Power System Manager

Analog Devices

3.0

Sequencing, monitoring, PEC

0 Kudos
Reply