Reduce Frequency of IMX93 by accesing resistors from userspace

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reduce Frequency of IMX93 by accesing resistors from userspace

770 次查看
dhruvinrajpura
Contributor III

I am using IMX93 EVK where I required to reduce cpu frequency of A core which is currently 1600MHz.

I want to reduce it up to 200MHz,

Earlier for IMX8ULP EVK I followed below method and I was able to control frequency on A core with accessing appropriate resisters

# Switch a35 to FRO 192 MHz
/unit_tests/memtool -32 0x292c0014=0x08000000

# Set PLLEN to 0
/unit_tests/memtool -32 0x292c0500=0x03000000

# Read and set the division and multiplication factors
/unit_tests/memtool -32 0x292c0014 1
/unit_tests/memtool -32 0x292c0510 1


# Set PLLEN to 1"
/unit_tests/memtool -32 0x292c0500=0x03000001

# Switch a35 to PLL2"
/unit_tests/memtool -32 0x292c0014=0x18000000

mhz

 
I checked reference manual of IMX93, but I am not able to get resistor by which I can control clock,

Can anyone guide me on this?

IMX93QSB 

标签 (3)
0 项奖励
回复
1 回复

749 次查看
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

CPU Frequency is changed between Low Power Modes (ND, OD, etc.). Please refer to this post.

Regards

0 项奖励
回复