Receiver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Receiver

1,369 Views
Jordan1x
Contributor I

Hi everyone,

I’m new to RF design, and I recently stumbled across a chip that looks interesting: the MC33591FTA, a PLL‑tuned UHF receiver originally from NXP (also previously Freescale/Motorola).  I’m thinking about using it in a simple wireless data or remote‑control receiver project, and I’d appreciate feedback from anyone who’s used it before or knows RF layout better than I do.

I’m planning to build a small remote‑sensor receiver: some simple sensors (temperature, door switch, etc.) send RF data, and this MC33591-based board receives it and passes decoded data to a microcontroller or small computer. I’m hoping this could be useful for home automation or remote monitoring without using Wi‑Fi or more complex RF modules.

My test plan is to start with basic reception: hook up an antenna, power the IC with 5 V (as specified), then connect the digital output from the receiver to a microcontroller UART or GPIO to decode the data. I’d first try a basic OOK or ASK transmitter at 434 MHz (easy to build or buy) for testing.

I also want to pay close attention to RF layout: antenna placement, matching, ground plane, and shielding to avoid noise and get decent sensitivity.
Because 315 / 434 MHz bands are shared by many devices, interference could also be an issue, I plan to test with different antennas and possibly filtering if needed.

For a simple home or hobby‑level installation: what size and type of antenna worked well for you (PCB trace antenna, whip, quarter‑wave, etc)? Any good reference for a matching network or layout guidelines for UHF small receivers using this chip?

Thanks in advance for any tips, suggestions, or warnings.

0 Kudos
Reply
1 Reply

1,317 Views
sofiaurueta
NXP Employee
NXP Employee

Hello,
Hope you are doing well!

 

I apologize for the inconveniences, but this device is no longer manufactured or recommended for new designs, and there is no support for it.

 

Alternatively, what we can offer is our sub-GHz wireless solutions, more information can be found here: Sub-GHz ISM Bands | NXP Semiconductors

 

Best regards,
Ana Sofia.

0 Kudos
Reply