[RW612][Rachio] Access Rights to J-link Flashloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[RW612][Rachio] Access Rights to J-link Flashloader

1,279件の閲覧回数
Masa1
NXP Employee
NXP Employee

From Customer, 

"We are having some issue with our Beta hardware, and we believe it is associated with the new flash chip that Ublox is using in their module. I was reading through the NXP document AN13869 which details how to create a custom flash configuration. There is a link in this document that points to the "NXP propriety J-Link flashloader source code" which appears to be the template I would need to work from. Unfortunately, when I click the link it says I do not have access. Can you please get me access to this file.
 
Here is the link:
 

"

Accounts that need access: 

Please let me know who I should reach out to to provide  RW612 access rights to the customer.

Thanks, 
Masa

ラベル(2)
0 件の賞賛
返信
1 返信

1,243件の閲覧回数
Masa1
NXP Employee
NXP Employee
Topic has been resolved.
0 件の賞賛
返信