RT600/700 GPIO Slew Rate Control

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT600/700 GPIO Slew Rate Control

2,025件の閲覧回数
aaronchin
Contributor II

Hi NXP,

In the RT600 and RT700 reference manual there is a GPIO setting to configure a GPIO's slew rate. This setting is either "disabled (default)" or "enabled." How is this setting tuning the internal driving circuit of the GPIO in its disabled and enabled state? 

434544897_2453569051697205_5100220487723441969_n.png434544897_2453569051697205_5100220487723441969_n.png

Best,

Aaron

ラベル(1)
0 件の賞賛
返信
1 返信

1,996件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Aaron,

as a part of MCUxpresso Config Tools, there is Pin tool available. The tool allows to generate code for pin routing and also for electrical pin configuration.

MCUxpresso Config Tools can be downloaded as standalone tool or they are also integrated into MCUxpresso IDE.

Hope this help

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信