RT1176 Boot through LPUART1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1176 Boot through LPUART1

3,271件の閲覧回数
Engineer_xxx
Contributor II

Hello Team

I'm trying to use UART to communicate with the RT1176 MCU, using USB by using the LPUART pins below in the picture. 

Can I use USB 2.0 to UART MCP2200 chip for this task? Also is this chip supported from your software side? if not what you recommend please? 
Regarding the boot I'm trying to boot only using QSPI flash W25Q128JW. 

Big Thanks

Engineer_xxx_0-1732253385654.png

Engineer_xxx_1-1732253473056.pngEngineer_xxx_2-1732253498022.png

Engineer_xxx_3-1732253983245.png

 

 

0 件の賞賛
返信
5 返答(返信)

3,185件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

LPUART and USB can be used on serial downloader, in that mode you will be able to communicate with the bootloader of the device being able to write/erase flash however to enter boot you will manually need to input the parameters.
To boot from QSPI you will need to use internal boot or boot from fuses, more details on the boot process please refer to system boot chapter on the Reference Manual.

The boot_cfg and boot_mode pads are needed for the system to work properly as the bootloader takes the state of the pins at boot to have information of the boot device. Boot_cfg pins can be replaced by the fuses but I do not suggest burn fuses until you are completely sure of the configuration as fuses cannot be re-burning.

Best regards,
Omar

0 件の賞賛
返信

3,255件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi,

there is a reference design RT1176-EVK and the schematic can be downloaded. This might help.

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信

3,249件の閲覧回数
Engineer_xxx
Contributor II

Hello Marek

In the reference manual shows many options to boots from. For my design I want to boot only from QSPI, and as you can see from the attached picture below, it shows many resistors needs to be used and Im trying to make my circuit smaller. So Im trying to avoid this method and boot using QSPI only using UART. Please advice. 

Could you please remove my name from the previous replay.
Thanks ahead for your support

Engineer_xxx_0-1732286714024.png

Engineer_xxx_1-1732286892653.png

 

 

0 件の賞賛
返信

3,240件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi,

sorry, I'm not HW engineer, so I cannot help more. You posted your question about "RT11xx" processor to forum related for "MCX" family of microcontrollers. I'd recommend posting to forum for i.MX RT1xxx processors, maybe someone can help there.

I removed your name from previous post.

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button

3,236件の閲覧回数
Engineer_xxx
Contributor II
Thanks Marek
0 件の賞賛
返信