[RT1170]: Debug or Flashing Issue with RT1170EVKB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[RT1170]: Debug or Flashing Issue with RT1170EVKB

357 Views
Rathore-pioneer
Contributor II

I was debugging a program on RT1170EVKB It was working fine.
While flashing another program something went wrong and then onwards, I am getting the following errors:

Rathorepioneer_0-1749707925566.png

 

Error logs:

LinkServer RedlinkMulti Driver v24.12 (Dec 18 2024 18:34:07 - crt_emu_cm_redlink build 869)

Found chip XML file in D:/2w-Display/NXP/project_workspace/evkbmimxrt1170_hello_world_cm7/Debug\MIMXRT1176xxxxx.xml

( 5) Remote configuration complete

Reconnected to existing LinkServer process.

============= SCRIPT: RT1170_connect_M7_wake_M4.scp =============

RT1170 Connect M7 and Wake M4 Script

DpID = 6BA02477

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

Setting M4 spin code

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

Setting M4 clock

Error: Wire Ack Fault - target connected?

Resetting M4 core

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

View cores on the DAP AP

DpID = 6BA02477

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

============= END SCRIPT ========================================

Probe Firmware: MCU-LINK on-board (r0E2) CMSIS-DAP V2.250 (NXP Semiconductors)

Serial Number: ZGSBFPW3SE32P

VID:PID: 1FC9:0143

USB Path: \\?\hid#vid_1fc9&pid_0143&mi_00#7&26a9c899&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}

Using memory from core 0 after searching for a good core

Using memory from core 0 after searching for a good core

Using memory from core 0 after searching for a good core

connection failed - Nn(05). Wire ACK Fault in DAP access.. Retrying

Using memory from core 0 after searching for a good core

Using memory from core 0 after searching for a good core

Using memory from core 0 after searching for a good core

Failed on connect: Nn(05). Wire ACK Fault in DAP access

Connected&Reset. Was: NotConnected. DpID: 6BA02477. CpuID: 00000000. Info: <None>

Last stub error 0: OK

Last sticky error: 0x0 AIndex: 0

Debug bus selected: MemAp 0

DAP Speed test unexecuted or failed

Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.

(100) Target Operation Failed

error closing down debug session - Nn(05). Wire ACK Fault in DAP access

 



 

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

297 Views
Sam_Gao
NXP Employee
NXP Employee

Hi,

It seems something error about 'connection?',

Please try to check in doing power-off/on again, or use other USB Cable instead.

0 Kudos
Reply

353 Views
Rathore-pioneer
Contributor II

Here is the Board LED status:

WhatsApp Image 2025-06-12 at 11.37.56.jpeg

Tags (1)
0 Kudos
Reply