RT1061 can not run the program in spi nor flash but well debug in ram.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1061 can not run the program in spi nor flash but well debug in ram.

ソリューションへジャンプ
2,165件の閲覧回数
lsjshengll
Contributor II
I'm a beginner working on driving a LED driver chip via I2C with the RT1061. It runs fine in ram debug mode (LED lights up), but when using flexspi_flash_nor_debug, the hardware initialization fails both in IAR simulation or flashing with jflash. I can read the flash contents, so the code is loaded. I've checked extensively but can't find the cause. Could you please help? Thanks.
I'm using flexspi1, with code partially transplanted from the hello world example. 
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,045件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @lsjshengll ,

That should be the issue. If the external flash does not provide the DQS signal, the DQS pin of the MCU should be floated. It cannot be reused as other functions.

Best regards,
Gavin

元の投稿で解決策を見る

10 返答(返信)
2,158件の閲覧回数
lsjshengll
Contributor II

I encountered the same issue when using the RT1021 to light up an LED with a regular GPIO. I barely modified the example code, only changing the IO port. I used Keil, and the LED lights up fine in debug mode. However, when using the flexspi_flash_nor_debug, the LED won't light up.

0 件の賞賛
返信
2,108件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @lsjshengll ,

Thanks for your interest in NXP MIMXRT series!

May I ask if you are testing with the example in SDK and RT1060-EVK?

You mean:

- Use examples from SDK;
- The original flexspi_flash_nor_debug can run;
- Flexspi_flash_nor_debug can't run after modifying the IO port?

Is that the case? If there is a problem with my understanding, please help me point it out.

Bests,
Gavin

0 件の賞賛
返信
2,092件の閲覧回数
lsjshengll
Contributor II

Hi,@Gavin_Jia 

Thank you for your reply.

- Use examples from SDK;  (see below)
- The original flexspi_flash_nor_debug can run; (Yes)
- Flexspi_flash_nor_debug can't run after modifying the IO port?(I'm not sure)

by the way RT1011 sdk can debug in the nor flash.

 

I have tried various methods to set up the RT1061 project, including Keil and IAR. Using the MCUXpresso Config tool and doing modification with hello world SDK. All of them have the same issue. The latest Keil project (see attachment) was built with MCUXpress config. ​Only added the I2C chip's driver and the main application. 

This RT1061 board I got from my colleague, it can debug before. I change the flash to W25Q64 and do some test. 


When doing debug in flexspi_nor_flash, it often gets stuck at the following location.

/* invalidate D-Cache */ sets = (uint32_t)(CCSIDR_SETS(ccsidr)); do { ways = (uint32_t)(CCSIDR_WAYS(ccsidr)); do { SCB->DCISW = (((sets << SCB_DCISW_SET_Pos) & SCB_DCISW_SET_Msk) | ((ways << SCB_DCISW_WAY_Pos) & SCB_DCISW_WAY_Msk) ); #if defined ( __CC_ARM ) __schedule_barrier(); #endif } while (ways-- != 0U); } while(sets-- != 0U); __DSB();

 

 

0 件の賞賛
返信
2,087件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @lsjshengll ,

Do you mean the issue happened on the board when replaced the flash? Is it possible to debug normally before changing the flash? 

0 件の賞賛
返信
2,073件の閲覧回数
lsjshengll
Contributor II

@Gavin_Jia 

I remember there is another difference. I use the flexspi DQS pin(GPIO_SD_B1_05) as I2C_SDA(I didn't connect that pin to flash). I don't know if it will affect Flash.

0 件の賞賛
返信
2,046件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @lsjshengll ,

That should be the issue. If the external flash does not provide the DQS signal, the DQS pin of the MCU should be floated. It cannot be reused as other functions.

Best regards,
Gavin

2,028件の閲覧回数
lsjshengll
Contributor II

@Gavin_Jia 

I have another question: The DQS pin can be routed to two pins (GPIO_SD_B1_05, GPIO_AD_B1_09). Why does using GPIO_SD_B1_05 will affect Flash operation? How does the RT1061 initialization determine this behavior? Do both pins need to be floated? Thank you.

0 件の賞賛
返信
2,014件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @lsjshengll ,

The two optional pins of DQS are not used casually. BootROM supports the FlexSPI primary option and the second option, that is, it has two groups of options. The selection method is the configuration in BootCFG2 or eFuse. The default configuration is the primary option. 

It should be the FlexSPI primary option on your board, so the corresponding DQS can only be GPIO_SD_B1_05.

Gavin_Jia_1-1742278461843.png

 

Gavin_Jia_0-1742278307341.png

 

2,010件の閲覧回数
lsjshengll
Contributor II

@Gavin_Jia 

Thank you so much. I will do a test tonight.

0 件の賞賛
返信
2,078件の閲覧回数
lsjshengll
Contributor II

@Gavin_Jia 

Yes, but the replaced Flash model is the same. My colleague used this board for some test and the old flash contained his program. So I replaced it with an empty Flash and programmed my own code into it.

0 件の賞賛
返信
%3CLINGO-SUB%20id%3D%22lingo-sub-2062431%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERT1061%E3%81%AF%E3%80%81SPI%E3%82%84%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%E3%81%A7%E3%83%97%E3%83%AD%E3%82%B0%E3%83%A9%E3%83%A0%E3%82%92%E5%AE%9F%E8%A1%8C%E3%81%99%E3%82%8B%E3%81%93%E3%81%A8%E3%81%AF%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%9B%E3%82%93%E3%81%8C%E3%80%81RAM%E3%81%A7%E3%81%86%E3%81%BE%E3%81%8F%E3%83%87%E3%83%90%E3%83%83%E3%82%B0%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2062431%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CDIV%20class%3D%22%22%3E%E7%A7%81%E3%81%AF%E5%88%9D%E5%BF%83%E8%80%85%E3%81%A7%E3%80%81RT1061%E3%81%A7I2C%E7%B5%8C%E7%94%B1%E3%81%A7LED%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BC%E3%83%81%E3%83%83%E3%83%97%E3%82%92%E9%A7%86%E5%8B%95%E3%81%99%E3%82%8B%E3%81%93%E3%81%A8%E3%81%AB%E5%8F%96%E3%82%8A%E7%B5%84%E3%82%93%E3%81%A7%E3%81%84%E3%81%BE%E3%81%99%E3%80%82RAM%20%E3%83%87%E3%83%90%E3%83%83%E3%82%B0%20%E3%83%A2%E3%83%BC%E3%83%89%20(LED%20%E3%81%8C%E7%82%B9%E7%81%AF)%20%E3%81%A7%E3%81%AF%E6%AD%A3%E5%B8%B8%E3%81%AB%E5%8B%95%E4%BD%9C%E3%81%97%E3%81%BE%E3%81%99%E3%81%8C%E3%80%81flexspi_flash_nor_debug%20%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8B%E3%81%A8%E3%80%81IAR%20%E3%82%B7%E3%83%9F%E3%83%A5%E3%83%AC%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%A7%E3%82%82%20jflash%20%E3%81%A7%E7%82%B9%E6%BB%85%E3%81%97%E3%81%A6%E3%82%82%E3%83%8F%E3%83%BC%E3%83%89%E3%82%A6%E3%82%A7%E3%82%A2%E3%81%AE%E5%88%9D%E6%9C%9F%E5%8C%96%E3%81%8C%E5%A4%B1%E6%95%97%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%E3%81%AE%E5%86%85%E5%AE%B9%E3%82%92%E8%AA%AD%E3%81%BF%E5%8F%96%E3%82%8B%E3%81%93%E3%81%A8%E3%81%8C%E3%81%A7%E3%81%8D%E3%82%8B%E3%81%AE%E3%81%A7%E3%80%81%E3%82%B3%E3%83%BC%E3%83%89%E3%81%8C%E8%AA%AD%E3%81%BF%E8%BE%BC%E3%81%BE%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%E5%BA%83%E7%AF%84%E5%9B%B2%E3%81%AB%E3%83%81%E3%82%A7%E3%83%83%E3%82%AF%E3%81%97%E3%81%BE%E3%81%97%E3%81%9F%E3%81%8C%E3%80%81%E5%8E%9F%E5%9B%A0%E3%81%AF%E8%A6%8B%E3%81%A4%E3%81%8B%E3%82%8A%E3%81%BE%E3%81%9B%E3%82%93%E3%80%82%E5%8A%A9%E3%81%91%E3%81%A6%E3%82%82%E3%82%89%E3%81%88%E3%81%BE%E3%81%99%E3%81%8B%3F%E6%84%9F%E8%AC%9D%E3%80%82%3C%2FDIV%3E%3CDIV%20class%3D%22%22%3E%E7%A7%81%E3%81%AFflexspi1%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6%E3%81%8A%E3%82%8A%E3%80%81%E3%82%B3%E3%83%BC%E3%83%89%E3%81%AFhello%20world%E3%81%AE%E4%BE%8B%E3%81%8B%E3%82%89%E9%83%A8%E5%88%86%E7%9A%84%E3%81%AB%E7%A7%BB%E6%A4%8D%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FDIV%3E%3C%2FLINGO-BODY%3E%3CLINGO-LABS%20id%3D%22lingo-labs-2062431%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CLINGO-LABEL%3E%E3%83%96%E3%83%BC%E3%83%88ROM%7C%E3%83%96%E3%83%BC%E3%83%88%7C%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%3C%2FLINGO-LABEL%3E%3C%2FLINGO-LABS%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2062433%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3ART1061%E3%81%AF%E3%80%81spi%E3%81%A7%E3%82%82%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%E3%81%A7%E3%82%82%E3%83%97%E3%83%AD%E3%82%B0%E3%83%A9%E3%83%A0%E3%82%92%E5%AE%9F%E8%A1%8C%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%9B%E3%82%93%E3%81%8C%E3%80%81RAM%E3%81%A7%E3%81%86%E3%81%BE%E3%81%8F%E3%83%87%E3%83%90%E3%83%83%E3%82%B0%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2062433%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3E%3CSPAN%3ERT1021%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6%E9%80%9A%E5%B8%B8%E3%81%AEGPIO%E3%81%A7LED%E3%82%92%E7%82%B9%E7%81%AF%E3%81%95%E3%81%9B%E3%82%8B%E3%81%A8%E3%81%8D%E3%81%AB%E3%82%82%E5%90%8C%E3%81%98%E5%95%8F%E9%A1%8C%E3%81%8C%E7%99%BA%E7%94%9F%E3%81%97%E3%81%BE%E3%81%97%E3%81%9F%E3%80%82%E3%82%B5%E3%83%B3%E3%83%97%E3%83%AB%E3%82%B3%E3%83%BC%E3%83%89%E3%82%92%E3%81%BB%E3%81%A8%E3%82%93%E3%81%A9%E5%A4%89%E6%9B%B4%E3%81%9B%E3%81%9A%E3%80%81IO%E3%83%9D%E3%83%BC%E3%83%88%E3%82%92%E5%A4%89%E6%9B%B4%E3%81%97%E3%81%9F%E3%81%A0%E3%81%91%E3%81%A7%E3%81%99%E3%80%82Keil%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%BE%E3%81%97%E3%81%9F%E3%81%8C%E3%80%81%E3%83%87%E3%83%90%E3%83%83%E3%82%B0%E3%83%A2%E3%83%BC%E3%83%89%E3%81%A7%E3%81%AFLED%E3%81%8C%E5%95%8F%E9%A1%8C%E3%81%AA%E3%81%8F%E7%82%B9%E7%81%AF%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E3%81%9F%E3%81%A0%E3%81%97%E3%80%81flexspi_flash_nor_debug%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8B%E3%81%A8%E3%80%81LED%E3%81%AF%E7%82%B9%E7%81%AF%E3%81%97%E3%81%BE%E3%81%9B%E3%82%93%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3C%2FLINGO-BODY%3E