Program of RT1061 can not run with flexspi nor flash but well in ram.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program of RT1061 can not run with flexspi nor flash but well in ram.

583件の閲覧回数
lsjshengll
Contributor II
I'm a beginner working on driving a LED driver chip via I2C with the RT1061. It runs fine in ram debug mode (LED lights up), but when using flexspi_flash_nor_debug, the hardware initialization fails both in IAR simulation or flashing with jflash. I can read the flash contents, so the code is loaded. I've checked extensively but can't find the cause. Could you please help? Thanks.
I'm using flexspi1, with code partially transplanted from the hello world example. 

The keil program in the attachment zip. Thank you so much.
 
 
0 件の賞賛
返信
1 返信

551件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @lsjshengll ,

Thanks for your questions!

I noticed that you already have another identical thread, so we can keep synchronization in your other thread.

Thanks in advance!

Bests,
Gavin

0 件の賞賛
返信