Problems with using uuu to burn the system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with using uuu to burn the system

348件の閲覧回数
Zion
Contributor I

Hello, my board is the IMX8QXPC0MEK, and I downloaded LF_v6.6.52-2.2.0_images_IMX8QXPC0MEK. After setting the board to 1, 0, 0, 0 (SERIAL mode), I flashed it on my PC (Ubuntu x86). I only plugged a Type-C cable into J10 of the board, maintaining the voltage and current at 12V and 0.23A. When I typed uuu -lsusb, I saw the following:
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.201-0-g727fc2b

Connected Known USB Devices
Path Chip Pro Vid Pid BcdVersion Serial_no
======================================================================
1:13 MX8QXP SDPS: 0x1FC9 0x012F 0x0002 060B400E8296409

This indicates that uuu is recognized, but after typing sudo uuu uuu.auto, the following error still appears:
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.201-0-g727fc2b

Success 0 Failure 1

1:13-060B400 1/ 1 [HID(W): LIBUSB_ERROR_IO (-1)] SDPS: boot -f imx-boot-imx8qxpc0mek-sd.bin-flash

I'd like to ask the developers what the problem is with my operation and how to effectively resolve this error so that I can flash the system to the eMMC. I very much look forward to your response!

ラベル(1)
  • USB

0 件の賞賛
返信
5 返答(返信)

328件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi,

Are you using below boot mode?

 

Zhiming_Liu_3-1756954359067.png

Can you try to use sudo before uuu?


Best Regards,
Zhiming

0 件の賞賛
返信

318件の閲覧回数
Zion
Contributor I

Dear Zhiming_Liu
My current setup is as shown:

Zion_0-1756958378569.jpeg

I really can't find the problem, please help, thank you!

0 件の賞賛
返信

316件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi,

It seems that you are using i.MX8QXPB0 MEK,can you see 'Si B0 SECO' string around M.2 socket?

You can try to flash B0 binary in this demo image.

Zhiming_Liu_0-1756962164168.png



Best Regards,
Zhiming

0 件の賞賛
返信

313件の閲覧回数
Zion
Contributor I

Dear Zhiming_Liu
To be honest, I don't know how to distinguish between c0 and b0, so I took a picture to show you.

Zion_0-1756964754859.jpeg

 

0 件の賞賛
返信

306件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi,

The i.MX8QXPC0 MEK is not black. You can try to flash B0 image to verify if this is i.MX8QXPB0.

Best Regards,
Zhiming

0 件の賞賛
返信