Problems with using uuu to burn the system

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problems with using uuu to burn the system

324 次查看
Zion
Contributor I

Hello, my board is the IMX8QXPC0MEK, and I downloaded LF_v6.6.52-2.2.0_images_IMX8QXPC0MEK. After setting the board to 1, 0, 0, 0 (SERIAL mode), I flashed it on my PC (Ubuntu x86). I only plugged a Type-C cable into J10 of the board, maintaining the voltage and current at 12V and 0.23A. When I typed uuu -lsusb, I saw the following:
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.201-0-g727fc2b

Connected Known USB Devices
Path Chip Pro Vid Pid BcdVersion Serial_no
======================================================================
1:13 MX8QXP SDPS: 0x1FC9 0x012F 0x0002 060B400E8296409

This indicates that uuu is recognized, but after typing sudo uuu uuu.auto, the following error still appears:
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.201-0-g727fc2b

Success 0 Failure 1

1:13-060B400 1/ 1 [HID(W): LIBUSB_ERROR_IO (-1)] SDPS: boot -f imx-boot-imx8qxpc0mek-sd.bin-flash

I'd like to ask the developers what the problem is with my operation and how to effectively resolve this error so that I can flash the system to the eMMC. I very much look forward to your response!

标签 (1)
0 项奖励
回复
5 回复数

304 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi,

Are you using below boot mode?

 

Zhiming_Liu_3-1756954359067.png

Can you try to use sudo before uuu?


Best Regards,
Zhiming

0 项奖励
回复

294 次查看
Zion
Contributor I

Dear Zhiming_Liu
My current setup is as shown:

Zion_0-1756958378569.jpeg

I really can't find the problem, please help, thank you!

0 项奖励
回复

292 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi,

It seems that you are using i.MX8QXPB0 MEK,can you see 'Si B0 SECO' string around M.2 socket?

You can try to flash B0 binary in this demo image.

Zhiming_Liu_0-1756962164168.png



Best Regards,
Zhiming

0 项奖励
回复

289 次查看
Zion
Contributor I

Dear Zhiming_Liu
To be honest, I don't know how to distinguish between c0 and b0, so I took a picture to show you.

Zion_0-1756964754859.jpeg

 

0 项奖励
回复

282 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi,

The i.MX8QXPC0 MEK is not black. You can try to flash B0 image to verify if this is i.MX8QXPB0.

Best Regards,
Zhiming

0 项奖励
回复