PowerQuad corrupts memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PowerQuad corrupts memory

跳至解决方案
1,441 次查看
Peter19
Contributor II

I am running example frdmmcxn947_powerquad_cmsis and extended size a bit.

Now memory gets corrupted around the locals so it looks to me like powerquad writes outside the expected memory.

 

 

 

static void arm_mat_add_q31Example(void)
{
    uint32_t srcRows, srcColumns; /* Temporary variables */
    arm_status status;
    arm_matrix_instance_q31 addMatrixA31;
    arm_matrix_instance_q31 addMatrixB31;
    arm_matrix_instance_q31 addMatrixR;
    #define MATRIX_SIZE 32
    q31_t A31[MATRIX_SIZE]       = {1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, 16, 17, 18, 19, 20, 21, 22, 23, 24, 25, 26, 27, 28, 29, 30, 31, 32};
    q31_t B31[MATRIX_SIZE]       = {10, 20, 30, 40, 50, 60, 70, 80, 90, 100, 110, 120, 130, 140, 150, 160, 170, 180, 190, 200, 210, 220, 230, 240, 250, 260, 270, 280, 290, 300, 310, 320};
    q31_t addResult[MATRIX_SIZE] = {0};
    q31_t addRef[MATRIX_SIZE]    = {11, 22, 33, 44, 55, 66, 77, 88, 99, 110, 121, 132, 143, 154, 165, 176, 187, 198, 209, 220, 231, 242, 253, 264, 275, 286, 297, 308, 319, 330, 341, 352};
    uint16_t rows = MATRIX_SIZE;
    uint16_t cols = 1;

    /* Initialise Matrix Instance addMatrixM1 with numRows, numCols and data array(M1) */
    srcRows    = rows;
    srcColumns = cols;
    arm_mat_init_q31(&addMatrixA31, srcRows, srcColumns, A31);

    /* Initialise Matrix Instance addMatrixM1 with numRows, numCols and data array(M1) */
    srcRows    = rows;
    srcColumns = cols;
    arm_mat_init_q31(&addMatrixB31, srcRows, srcColumns, B31);

    /* Initialise Matrix Instance addMatrixM1 with numRows, numCols and data array(M1) */
    srcRows    = rows;
    srcColumns = cols;
    arm_mat_init_q31(&addMatrixR, srcRows, srcColumns, addResult);

    status = arm_mat_add_q31(&addMatrixA31, &addMatrixB31, &addMatrixR);
    EXAMPLE_ASSERT_TRUE(status == ARM_MATH_SUCCESS);

    for (uint32_t i = 0; i < MATRIX_SIZE; i++)
    {
        EXAMPLE_ASSERT_TRUE(addRef[i] == addMatrixR.pData[i]);
    }
}

 

 

 

 

标签 (3)
0 项奖励
回复
1 解答
1,415 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @Peter19 ,

Thanks for your post. The reason is that there are restrictions on the dimensions of the power_quad matrix operations. It only supports a maximum size of 16 * 16, and setting the row to 32 is not reasonable. You can find the detailed information in the Reference Manual. See the figure below.

Celeste_Liu_0-1736332255025.png

Hope it can help you.

BRs,

Celeste

--------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
--------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,416 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @Peter19 ,

Thanks for your post. The reason is that there are restrictions on the dimensions of the power_quad matrix operations. It only supports a maximum size of 16 * 16, and setting the row to 32 is not reasonable. You can find the detailed information in the Reference Manual. See the figure below.

Celeste_Liu_0-1736332255025.png

Hope it can help you.

BRs,

Celeste

--------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
--------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,404 次查看
Peter19
Contributor II
Hello @Celeste_Liu
It is not obvious to me that 32x1 is not supported since it is much smaller than 16x16...
Regards
/Peter
0 项奖励
回复
1,381 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @Peter19 ,

What I mean is that neither a single dimension of the matrix, be it the row or the column, can exceed 16. If you change 32x1 to 16x2, it will work. Similarly, I've tested the maximum size of 16x16 and there was no problem.

BRs,

Celeste

0 项奖励
回复