Optical microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Optical microcontroller

3,146件の閲覧回数
SheemaEgbert
Contributor I

Hi, 

I'm looking for a microcontroller with on-chip IDACs, support for thermoelectric cooler control, on-chip temperature sensing circuits etc., for use as an optical signal processor and controller. Could you suggest some possible NXP microcontrollers/microprocessors?

Thanks,

Sheema  

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

3,081件の閲覧回数
SheemaEgbert
Contributor I

Thanks, XianJun, this clears the part about the current DACs. 

0 件の賞賛
返信

3,110件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that all the on-chip DACs for MCU are voltage output DAC instead of current output DAC.

For you application of iDAC, you can use on-chip DAC of MCU to output voltage from DAC_OUTPUT pin, then connect the DAC_OUTPUT pin to an external OP AMP and a transistor/MOSFET to output current.

The MCXN fanily has 14 bits resolution on-chip voltage output DAC.

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

The other family, for example LPC84x low cost MCU also has on-chip voltage output DAC.

Hope it can help you

BR

XiangJun Rong