NFC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC

2,762件の閲覧回数
Khutwad
Contributor I

Hi,

do we need any approval from Apple for programing firmware on LPC82x series for NFC application.

 

 

 

Thanks

Ankush

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,707件の閲覧回数
Khutwad
Contributor I

WhatsApp Image 2025-04-28 at 15.03.42_b30ed281.jpgWhatsApp Image 2025-04-28 at 15.03.42_b30ed281.jpg

タグ(1)
0 件の賞賛
返信

2,694件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

 ECP is a proprietary extension developed by Apple. You need to get approval from Apple.

0 件の賞賛
返信

2,564件の閲覧回数
Khutwad
Contributor I

do we need to put any code for ECP in firmware code? if not going anything why we need approval ?

0 件の賞賛
返信

2,521件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You only need to integrate the ECP code when your NFC device needs to perform  ​mutual authentication with the Apple SE chip.

For more, I suggest you check with Apple directly.

0 件の賞賛
返信

2,747件の閲覧回数
AshutoshNama
Contributor III

Hey Khutwad,

Good question! 
You don’t need any special approval from Apple just to program firmware on the LPC82x series for your NFC application — as long as you’re using standard NFC communication.

Now, if you plan to talk to iPhones in a normal way (like basic NFC tag reading), you’re totally fine. No permissions, no Apple paperwork. 
But, if your application is trying to do something extra fancy — like deep integration with iOS, accessing special NFC features, or if you want to slap a "Made for iPhone" (MFi) badge on your product — then yes, you’d need to join Apple’s MFi Program. (It’s a bit of a process but nothing too scary.)

Bottom line:
Normal NFC use? → You're good to go! 
Special iPhone magic or branding? → Might need MFi approval.

Hope that clears it up! Let me know if you want a quick cheat sheet on what counts as "standard NFC" vs "MFi NFC." Could save you some headaches later. 

Best Regards,
Ashutosh

0 件の賞賛
返信