NFC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC

2,749 Views
Khutwad
Contributor I

Hi,

do we need any approval from Apple for programing firmware on LPC82x series for NFC application.

 

 

 

Thanks

Ankush

Labels (1)
0 Kudos
Reply
5 Replies

2,694 Views
Khutwad
Contributor I

WhatsApp Image 2025-04-28 at 15.03.42_b30ed281.jpgWhatsApp Image 2025-04-28 at 15.03.42_b30ed281.jpg

0 Kudos
Reply

2,681 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

 ECP is a proprietary extension developed by Apple. You need to get approval from Apple.

0 Kudos
Reply

2,551 Views
Khutwad
Contributor I

do we need to put any code for ECP in firmware code? if not going anything why we need approval ?

0 Kudos
Reply

2,508 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You only need to integrate the ECP code when your NFC device needs to perform  ​mutual authentication with the Apple SE chip.

For more, I suggest you check with Apple directly.

0 Kudos
Reply

2,734 Views
AshutoshNama
Contributor III

Hey Khutwad,

Good question! 
You don’t need any special approval from Apple just to program firmware on the LPC82x series for your NFC application — as long as you’re using standard NFC communication.

Now, if you plan to talk to iPhones in a normal way (like basic NFC tag reading), you’re totally fine. No permissions, no Apple paperwork. 
But, if your application is trying to do something extra fancy — like deep integration with iOS, accessing special NFC features, or if you want to slap a "Made for iPhone" (MFi) badge on your product — then yes, you’d need to join Apple’s MFi Program. (It’s a bit of a process but nothing too scary.)

Bottom line:
Normal NFC use? → You're good to go! 
Special iPhone magic or branding? → Might need MFi approval.

Hope that clears it up! Let me know if you want a quick cheat sheet on what counts as "standard NFC" vs "MFi NFC." Could save you some headaches later. 

Best Regards,
Ashutosh

0 Kudos
Reply