MPC8378

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8378

2,950 Views
YPKEJI12341
Contributor I

MPC8378配套使用的镁光存储型号为MT47H64M16HR-25EIT:H,因为原型号停产,现在更换型号为MT47H64M16NF-25EIT:M,动态随机存取存储器型号IS43DR16640C-25DBLI,其他物料没有更换,生产调试发现之前的程序不管怎么调试都无法正确读取数据,数据报错,比如程序写的1111,数据读取的是1100,请问我们适配程序应该怎么调整?

 

微信图片1.png微信图片2.png

 

0 Kudos
Reply
5 Replies

2,745 Views
YPKEJI12341
Contributor I

这个是原理图

全部原理图.jpg

0 Kudos
Reply

2,901 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

If you have the issues with the new dram could be any issue with the timing parameters as you are facing data corruption.

Please verify the main difference between both DDR and Verify DDR Timing Parameters to adjust all the values and perform Memory Stress Tests.

0 Kudos
Reply

2,808 Views
YPKEJI12341
Contributor I

Does DDR refer to Micron chips?
Does verify DDR refer to ISSI chips?

0 Kudos
Reply

2,702 Views
Oswalag
NXP TechSupport
NXP TechSupport

Yes, DDR mean SDRAM chips from Micron. Small differences in silicon revisions or internal timing can cause compatibility issues, you have to compare and adjust the timing parameters according to both datasheets and update the memory controller initialization code, and run memory test to validate the configuration. 

0 Kudos
Reply

2,745 Views
YPKEJI12341
Contributor I
MPC8378配套使用的镁光存储型号为MT47H64M16HR-25EIT:H,因为原型号停产,现在更换型号为MT47H64M16NF-25EIT:M,其他物料没有更换,生产调试发现之前的程序不管怎么调试都无法正确读取数据,数据报错,比如程序写的1111,数据读取的是1100,请问我们适配程序应该怎么调整?
0 Kudos
Reply