MIMXRT1171CVM8A Dummy Read Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1171CVM8A Dummy Read Error

974件の閲覧回数
SheremyHsu
Contributor I

Hi NXP team,

I currently have a system using the MIMXRT1171CVM8A for booting, but it is unable to boot successfully. The boot log shows the following dummy read error. Could you please explain what dummy read is and what could be the cause of the error?


[00000.044] [00:05:40] ERROR - Dummy read publish return unexpected value 0xbdcdbad3
[00000.044] [00:05:40] INFO - prev write addr 0xbf587060c, pulish status history: [0xadc00000, 0x0])
[00000.044] [00:05:40] ERROR - metric_spi_master_error -"op":"read","addr":"0xbf0587060c","data":"0x400","status":1

SheremyHsu_0-1734089285509.pngSheremyHsu_0-1734089285509.png

Thank you!

0 件の賞賛
返信
1 返信

932件の閲覧回数
Sam_Gao
NXP Employee
NXP Employee

Hi @SheremyHsu 

Would you please clairfy more details to help us understand about this issue? such as which tool/version are you using? what about Hardware connection when issue happen? reproduce steps, etc.

0 件の賞賛
返信