MIMXRT1171CVM8A Dummy Read Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1171CVM8A Dummy Read Error

556 Views
SheremyHsu
Contributor I

Hi NXP team,

I currently have a system using the MIMXRT1171CVM8A for booting, but it is unable to boot successfully. The boot log shows the following dummy read error. Could you please explain what dummy read is and what could be the cause of the error?


[00000.044] [00:05:40] ERROR - Dummy read publish return unexpected value 0xbdcdbad3
[00000.044] [00:05:40] INFO - prev write addr 0xbf587060c, pulish status history: [0xadc00000, 0x0])
[00000.044] [00:05:40] ERROR - metric_spi_master_error -"op":"read","addr":"0xbf0587060c","data":"0x400","status":1

SheremyHsu_0-1734089285509.png

Thank you!

0 Kudos
Reply
1 Reply

514 Views
Sam_Gao
NXP Employee
NXP Employee

Hi @SheremyHsu 

Would you please clairfy more details to help us understand about this issue? such as which tool/version are you using? what about Hardware connection when issue happen? reproduce steps, etc.

0 Kudos
Reply