MCXN947 SDK documentation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCXN947 SDK documentation

1,881 Views
stevenlutz
Contributor III

Where is the full sdk documentation located for the MCXN947 when using mcuxpresso? 

It seems all the versions that I find online are very old. 

Thank you. 

Labels (2)
Tags (1)
0 Kudos
Reply
7 Replies

1,826 Views
stevenlutz
Contributor III

I'm using
MCUXpresso IDE v24.9 [Build 25] [2024-09-26]
SDK v 2.26.1

I have opened the link to the SDK at https://mcuxpresso.nxp.com/mcuxsdk/latest/html/index.html However, I don't see where the relevant documentation for the flexcan peripherals is located. 
Searching for flexcan in the search bar only returns flexcan examples and doesn't actually return flexcan SDK documentation. 

This newer layout of the SDK docs is harder to find whats needed than the older version from a few years ago. 

 

 

0 Kudos
Reply

1,793 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @stevenlutz ,

I noticed that you mentioned using SDK v 2.26.1. I believe it might be a typo on your part, as the only version we have is v 2.16.1.
In the SDK documentation of version 2.16.1, you can find some APIs related to flexcan, as shown in the figure below.

Celeste_Liu_0-1737603361572.png

Regarding the issue you mentioned that the layout of the new v24.12 SDK documentation is not user-friendly, thank you for your feedback. I will forward it to the relevant team so that they can improve the product in the future and enhance your experience.

BRs,

Celeste

 

0 Kudos
Reply

1,781 Views
stevenlutz
Contributor III

I found the link to the SDK reference manual, I was overlooking it in the list in the MCUxpresso SDK menu. I believe this is going to be very helpful, however the online SDK link mentioned earlier is the one that I have trouble with... it's very strange. 


thanks again. 

0 Kudos
Reply

1,776 Views
Celeste_Liu
NXP Employee
NXP Employee

I'm glad that you've found the documentation you needed. Regarding your feedback on the online SDK link, I've already submitted it to the relevant team via Jira. Here is the Jira ticket number: MCUX-76108.

0 Kudos
Reply

1,875 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @stevenlutz ,

Thanks for your post. Please refer to the following method to open the SDK documentation:

On the "installed SDKs" page, locate the SDK of SDK_2.x_FRDM-MCXN947. Then, right - click the mouse and select "SDK documentation".

Celeste_Liu_0-1737367886783.png

 

Hope it can help you.

BRs,

Celeste

--------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
--------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,870 Views
stevenlutz
Contributor III

I searched there and I don't see a document that includes the flexcan and usb peripherals. Only specific thi gs thats dont apply to me. Isn't there a comprehensive guide to the entire sdk? 

0 Kudos
Reply

1,847 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello,

I had a look and could see the flexcan and usb peripherals. I'm using MCUXpresso version 24.9, with SDK version 2.16. Could you please let me know the versions of the IDE and SDK you are using?

Or you can directly get the documentation of the latest version of the SDK in the following way.

1. Open SDK download link:
Select Board | MCUXpresso SDK Builder

2. Search "MCXN947", select the latest SDK version 24.12 and click "BUILD SDK".

Celeste_Liu_0-1737369307887.png

3. Select the middleware you need, and then click "BUILD SDK".

Celeste_Liu_1-1737369438672.png

4. Click "Download", then click "MCUXpresso SDK Documentation".

Celeste_Liu_2-1737369562511.pngCeleste_Liu_3-1737369598374.png

5. The documentation of the latest SDK can be seen in the form of a web link.

Celeste_Liu_4-1737369680864.png

Hope it can help you.

BRs,

Celeste

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply