MCXN235 Debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCXN235 Debug

1,596件の閲覧回数
linsy
Contributor II

When we use the SDK code of MCXN235 to debug on our MCXN235 board, an error occurs and the error message reads: "Break at address '0x20018040' with no debug information available, or outside of program code." However, if we swap the MCXN235 chip on our board with the MCXN236 development board chip, the board can be debugged normally and the development board will encounter the same problem.

May I ask if this is a configuration issue with the MCXN235 software? Or there is a problem with the bootloader. The code used is the default version of the SDK

我们用MCXN235的SDK代码 在我们MCXN235板子上 debug时会出错,报错内容为 “Break at address '0x20018040' with no debug information available ,or outside of program code.”. 但是如果我们把我们板子的MCXN235芯片和MCXN236开发板芯片交换之后,我们板子就能正常debug了,开发板就会出现同样的问题

请问下这个是MCXN235软件哪里配置问题吗?或者引导程序有问题 代码用的是SDK默认的

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,588件の閲覧回数
linsy
Contributor II

024b63502d8e009289fb7a7f8b2140b4.png024b63502d8e009289fb7a7f8b2140b4.png

c5cca847196e1faf8721d3448d0c12bd_compress.jpgc5cca847196e1faf8721d3448d0c12bd_compress.jpg

0 件の賞賛
返信

1,573件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi @linsy 

 

我看到您在private ticket里提交了同样的问题,我已经回复您,请查看。

有任何问题及时联系我们。谢谢!

 

BR

Alice

0 件の賞賛
返信