MCXA156VLH (LQFP64 version) availability

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCXA156VLH (LQFP64 version) availability

跳至解决方案
336 次查看
rj_engineer
Contributor III

The VLH (LQFP64 version) of the MCXA154 to MCXA156 is listed on the datasheet but not on the "Buy/parametric" view on the MCXA webpage.

 

Therefore, is this package available for the MCXA154 to MCXA156 with the same longevity as other packages?

标签 (1)
0 项奖励
回复
1 解答
319 次查看
Habib_MS
NXP Employee
NXP Employee

Hi @rj_engineer,
Is this package available for the MCXA154 to MCXA156 with the same longevity as other packages?

Yes, all MCXA15x devices currently share the same product longevity status, as illustrated in the image below:

Habib_MS_0-1750109578241.png

This image was sourced from the official product longevity page.
BR
Habib

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
320 次查看
Habib_MS
NXP Employee
NXP Employee

Hi @rj_engineer,
Is this package available for the MCXA154 to MCXA156 with the same longevity as other packages?

Yes, all MCXA15x devices currently share the same product longevity status, as illustrated in the image below:

Habib_MS_0-1750109578241.png

This image was sourced from the official product longevity page.
BR
Habib

 

0 项奖励
回复