MCXA156VLH (LQFP64 version) availability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCXA156VLH (LQFP64 version) availability

Jump to solution
985 Views
rj_engineer
Contributor III

The VLH (LQFP64 version) of the MCXA154 to MCXA156 is listed on the datasheet but not on the "Buy/parametric" view on the MCXA webpage.

 

Therefore, is this package available for the MCXA154 to MCXA156 with the same longevity as other packages?

Labels (1)
0 Kudos
Reply
1 Solution
968 Views
Habib_MS
NXP Employee
NXP Employee

Hi @rj_engineer,
Is this package available for the MCXA154 to MCXA156 with the same longevity as other packages?

Yes, all MCXA15x devices currently share the same product longevity status, as illustrated in the image below:

Habib_MS_0-1750109578241.png

This image was sourced from the official product longevity page.
BR
Habib

 

View solution in original post

0 Kudos
Reply
1 Reply
969 Views
Habib_MS
NXP Employee
NXP Employee

Hi @rj_engineer,
Is this package available for the MCXA154 to MCXA156 with the same longevity as other packages?

Yes, all MCXA15x devices currently share the same product longevity status, as illustrated in the image below:

Habib_MS_0-1750109578241.png

This image was sourced from the official product longevity page.
BR
Habib

 

0 Kudos
Reply