MCUXpresso eDMA use with LPI2C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso eDMA use with LPI2C

1,477件の閲覧回数
rantonetti
Contributor I

This is a general question.

I have looked at the NXP provided edma slave board to board example project provided for the imxrt1050-evkb.

This project does not use the MCUXpresso peripheral configuration tool.

I have attempted to set the edma up for use with the lpi2c and I can't seem to get the edma working.

Is there a reason NXP did not enable the peripheral configuration tools for this demo?

It's seems as though all set up is done manually.

I seem to remember reading somewhere that if MCUXpresso manages the peripherals that the clock configuration will stop edma from working.

If you are reading this and you are with NXP can you provide a reference on how to get this working with the config tool?

ラベル(1)
0 件の賞賛
返信
1 返信

1,432件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @rantonetti,

I wouldn't be able to say with certainty when (or if) the SDK team will fully implement the example codes with Peripherals Tool. But for now, the evkbimxrt1050_lpi2c_edma_b2b_transfer example projects, like the rest of the evkbimxrt1050 demos, are fully integrated with at least Pins and Clocks Tool.

What errors do you see when setting up the eDMA on Peripherals Tool?

BR,
Edwin.

0 件の賞賛
返信