How maximum size of RT1050 External SDRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How maximum size of RT1050 External SDRAM

跳至解决方案
2,588 次查看
abs_setian
Contributor II

Hello Im using RT1050 NXP chip

And I need 128MB QSPI Flash memory and 128MB SDRAM.

Is it possible to using 128MB SDRAM?

I wish to use 32MB SDRAM x 4 CS.

I wanna know how to configuration those settings( Hardware and Software ).

Is there any manual for setting external RAM? 

I read reference manual(SEMC). but I didn't undeerstand..

I need more sepcific tutorial for using more than 3 chip select for extenral RAM

 

Thanks for reading

标签 (1)
0 项奖励
回复
1 解答
2,532 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

SEMC of RT1050 supports 4 Chip Select (CS) each CS supports up to 64MB. Unfortuanately, there is no detailed guide besides the  SDK examples, you might refer to the RT1170 example since the EVK connects two SDRAMs.

You need to connect every buses and signals between RAM chips but exclude only CS signals, because CS should be connected independently.

Best regards,
Omar

在原帖中查看解决方案

2 回复数
2,533 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

SEMC of RT1050 supports 4 Chip Select (CS) each CS supports up to 64MB. Unfortuanately, there is no detailed guide besides the  SDK examples, you might refer to the RT1170 example since the EVK connects two SDRAMs.

You need to connect every buses and signals between RAM chips but exclude only CS signals, because CS should be connected independently.

Best regards,
Omar

2,519 次查看
abs_setian
Contributor II

Thanky you!!

0 项奖励
回复