MCSA with PowerQuad

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCSA with PowerQuad

2,059 Views
erikraynolds
Contributor IV

Hello,

 

Is it possible to use PowerQuad DSP Coprocessor for motor current signature analysis - FFT based ?

Any example  of phase current FFT effectivnes with PowerQuad on 3 phase currents?

 

Thanks.

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,025 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello ,

Thanks for contacting NXP Tech Support. I am here to support you.

[Q1] Is it possible to use PowerQuad DSP Coprocessor for motor current signature analysis - FFT based ?

[A1] Yes, it is possible. 

[Q2] Any example of phase current FFT effectivnes with PowerQuad on 3 phase currents?

[A2] The frdmmcxn947_powerquad_benchmark_fft demo could be a useful reference for your questions.  By converting and inputting your three-phase current data into an appropriate format, it may meet your needs. 

To get the demo, download the FRDM-MCXN947 SDK. Refer to Importing an SDK Package into MCUXpresso IDE  and install it in MCUXpresso. Open it as below picture shows.

Celeste_Liu_0-1730097168096.pngCeleste_Liu_0-1730097168096.png

Hope the above information is helpful to you.

BR,

Celeste

0 Kudos
Reply

2,018 Views
erikraynolds
Contributor IV
Can it handle 3 Current content in real time?
0 Kudos
Reply

2,012 Views
Celeste_Liu
NXP Employee
NXP Employee

Hi,

The PowerQuad DSP coprocessor integrated with the NXP MCX N series has the potential for real-time three current analysis, but this indeed depends on multiple factors.

The real-time data processing capability of the system is affected by many aspects, including the sampling rate and resolution of the ADC used for current signal acquisition, the computational complexity and efficiency of the FFT algorithm, system latency including data acquisition, processing, output or control operations, and the clock speed and available resources of the microcontroller with the PowerQuad coprocessor.

Regarding the PowerQuad DSP parameters in the MCX Nx4x series, you can refer to "Chapter 18 PowerQuad DSP Coprocessor and Accelerator" in MCXNx4xRM.

BR,

Celeste

0 Kudos
Reply