MCSA with PowerQuad

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCSA with PowerQuad

2,100件の閲覧回数
erikraynolds
Contributor IV

Hello,

 

Is it possible to use PowerQuad DSP Coprocessor for motor current signature analysis - FFT based ?

Any example  of phase current FFT effectivnes with PowerQuad on 3 phase currents?

 

Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,066件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello ,

Thanks for contacting NXP Tech Support. I am here to support you.

[Q1] Is it possible to use PowerQuad DSP Coprocessor for motor current signature analysis - FFT based ?

[A1] Yes, it is possible. 

[Q2] Any example of phase current FFT effectivnes with PowerQuad on 3 phase currents?

[A2] The frdmmcxn947_powerquad_benchmark_fft demo could be a useful reference for your questions.  By converting and inputting your three-phase current data into an appropriate format, it may meet your needs. 

To get the demo, download the FRDM-MCXN947 SDK. Refer to Importing an SDK Package into MCUXpresso IDE  and install it in MCUXpresso. Open it as below picture shows.

Celeste_Liu_0-1730097168096.png

Hope the above information is helpful to you.

BR,

Celeste

0 件の賞賛
返信

2,059件の閲覧回数
erikraynolds
Contributor IV
Can it handle 3 Current content in real time?
0 件の賞賛
返信

2,053件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hi,

The PowerQuad DSP coprocessor integrated with the NXP MCX N series has the potential for real-time three current analysis, but this indeed depends on multiple factors.

The real-time data processing capability of the system is affected by many aspects, including the sampling rate and resolution of the ADC used for current signal acquisition, the computational complexity and efficiency of the FFT algorithm, system latency including data acquisition, processing, output or control operations, and the clock speed and available resources of the microcontroller with the PowerQuad coprocessor.

Regarding the PowerQuad DSP parameters in the MCX Nx4x series, you can refer to "Chapter 18 PowerQuad DSP Coprocessor and Accelerator" in MCXNx4xRM.

BR,

Celeste

0 件の賞賛
返信