MC33772C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33772C

Jump to solution
1,236 Views
kevinyuee
Contributor III

Hi,
   I hope to provide an initialization register writing instruction(such as 00 00 00 01 31 7B) 
and a corresponding register reading instruction so that I can confirm that my communication is working.
Thanks a lot!

Labels (1)
0 Kudos
Reply
1 Solution
1,220 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @kevinyuee ,

Thanks for your post. The MC33772C is not belong to MCXC series. So this is not the right channel to post.

I suggest you create a new post on:

High Performance Analog Front End Interfaces - NXP Community

The support engineer there will help you further.

BRs,

Celeste

View solution in original post

0 Kudos
Reply
1 Reply
1,221 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @kevinyuee ,

Thanks for your post. The MC33772C is not belong to MCXC series. So this is not the right channel to post.

I suggest you create a new post on:

High Performance Analog Front End Interfaces - NXP Community

The support engineer there will help you further.

BRs,

Celeste

0 Kudos
Reply