MC33772C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,234件の閲覧回数
kevinyuee
Contributor III

Hi,
   I hope to provide an initialization register writing instruction(such as 00 00 00 01 31 7B) 
and a corresponding register reading instruction so that I can confirm that my communication is working.
Thanks a lot!

ラベル(1)
0 件の賞賛
返信
1 解決策
1,218件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @kevinyuee ,

Thanks for your post. The MC33772C is not belong to MCXC series. So this is not the right channel to post.

I suggest you create a new post on:

High Performance Analog Front End Interfaces - NXP Community

The support engineer there will help you further.

BRs,

Celeste

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,219件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @kevinyuee ,

Thanks for your post. The MC33772C is not belong to MCXC series. So this is not the right channel to post.

I suggest you create a new post on:

High Performance Analog Front End Interfaces - NXP Community

The support engineer there will help you further.

BRs,

Celeste

0 件の賞賛
返信