Looking for eIQ command line tool to convert TFlite mode to the NPU of MCXN947

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Looking for eIQ command line tool to convert TFlite mode to the NPU of MCXN947

1,293 次查看
ramkumarkoppu_p
Contributor III

Hi,

I remember there is used to be command line converter tool to convert TFlite model to utilise the operators available on the NPU of MCXN947, now couldn't find this tool on the NXP website. can you help to me find and download this command line to use it both Ubuntu 22.04 and apple silicon Mac please?

标签 (2)
标记 (1)
0 项奖励
回复
1 回复

1,251 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @ramkumarkoppu_p 

You can download the eIQ® Toolkit from the below link.

eIQ® Toolkit | NXP Semiconductors

HangZhang_0-1729496609168.png

It includes the MODEL TOOL and COMMAND LINE.

BR

Hang

0 项奖励
回复