IMx.6Q IBIS model ENET pins voltage reference

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMx.6Q IBIS model ENET pins voltage reference

1,030 Views
Mathiyazhagan
Contributor I

Hi Team,

We are using MCIMX6Q5EYM10AE in our design. For SI simulation, we are downloading IBIS model from NXP website.

While assigning models to ENET_MDC & ENET_MDIO pins voltage reference for that pins shows 3.3V, 1.8V and 1.2V models only.
But actual pin voltage which we have used is 2.5V.
As per datasheet that pin Min.voltage is 1.65V.

Mathiyazhagan_0-1737635292426.png

Mathiyazhagan_1-1737635430257.png



Need a update on that specific pin voltage models in the IBIS models.

 

0 Kudos
Reply
1 Reply

990 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Mathiyazhagan 

I hope you are doing very well.

 

The signal you are looking on Datasheet is NVCC_ENET, that is the "power rail" for ENET module.

ENET_MDC and ENET_MDIO are functional pads, that can works at 3.3 and 1.8.

The IBIS is correct.

 

Best regards,

Salas.

0 Kudos
Reply