Help with MaaxBoard i.MX93 Pinout, GPIO Configuration (Input/Output), and Timer Setup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Help with MaaxBoard i.MX93 Pinout, GPIO Configuration (Input/Output), and Timer Setup

517 次查看
Manjunathb
Contributor II

Hi everyone,

I’m currently working with the MaaxBoard based on the NXP i.MX93 processor, and I need some guidance on the following:

  1. MaaxBoard Pinout Diagram:

    • Where can I find the official pinout mapping (board headers vs. SoC pins)?

    • Specifically looking for GPIO-capable pins and alternate functions like PWM, I2C, SPI, etc.

  2. GPIO Configuration (Input/Output):

    • What is the correct method to configure GPIOs in i.mx93 cortex-m33 for input/output on MaaxBoard i.MX93?

    • Timer Configuration Using GPIO Pin:

      • I want to use a timer/counter (like PWM or capture input) mapped to a GPIO pin.

      • How can I configure a GPIO pin for PWM output or input capture?

      • Do I need to modify the device tree or use existing kernel modules?

Any reference to:

  • Working device tree snippets

  • GPIO pin number mapping (Maax header to i.MX93 ball name)

  • PWM/timer configuration examples
    would be greatly appreciated.

Thanks in advance!

i.MX93 

标签 (2)
0 项奖励
回复
2 回复数

473 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi  Manjunathb

 

The MaaxBoard is manufactured and supported by Element14 , I would suggest you to reach out the owner so they maybe able to provide more insights on their BSP and their board.

 

MaaXBoard OSM93 - element14 Community

MaaXBoard Hardware Design - element14 Community

 

For NXP's EVK,  we use SDK to configure the GPIO.  like below

danielchen_0-1753509413519.png

 

For the IOMUX alternate functions for i.MX93, 

danielchen_1-1753509648541.png

 

Please contact the owner of this board for better help.

 

Regards

Daniel

0 项奖励
回复

469 次查看
Manjunathb
Contributor II
okay thank you for your response!
0 项奖励
回复