Freemaster Communication with Labview

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freemaster Communication with Labview

1,248件の閲覧回数
mich28
Contributor II

Hello Community, I implemented and used the "mcbcom.dll" library with python 3.9 64 bit and now I can use it. Out of necessity I start using the same library with the "Call Library Function" on Labview 32bit 2015 but I continue to receive errors. I was wondering if anyone has already used this library and if this library is really 32bit as written in many forums, I tried to use it with python 3.13 32 bit and it doesn't work....has anyone had the same problem?

MCU:     LPC5536JBD100

ラベル(1)
0 件の賞賛
返信
1 返信

1,227件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi mich28,

Freemaster is NXP's system debug tool and it doesn't have the feature of directly supporting Labview communication.
There may be some indirect methods. For example, Freemaster can transfer MCU data to LabView via UART. But we don't have demo on this becuase LabView is not NXP prodcut.

Let's leave your question here, if other users have experiences about it, welcome to share.

Have a nice day,

Jun Zhang

0 件の賞賛
返信