FRDM-RW612 Error: Verification failed @ address 0x18000000

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-RW612 Error: Verification failed @ address 0x18000000

12,830 Views
nguterresn
Contributor II

Hey!

I've been trying to make the FRDM RW612 work. I was able to flash for a couple of times, until I've connected the Adafruit TFT 2.8 LCD screen on top of the Arduino Header presented in the board, and, after that, I was able to flash a few more times until something went wrong and I couldn't anymore.

I've tried everything at this points:

- Downloaded MCUExpresso, created a default build for the board and tried to flash: failed.

- Downloaded the LinkServer, change from JLink probe to CMSIS, tried to flash: failed.

- Played around with JLink console: I can read and write onto specific addresses, but I can't flash.

I've tried different builds, NXP examples and Zephyr samples (Blinky): does't work.

Here's an example of error message from JLink:

 

 

 

J-Link>loadfile /Users/nunoguterres/Downloads/zephyr.elf 0x18000000
'loadfile': Performing implicit reset & halt of MCU.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
  MSPLIM cleared
ResetTarget() end - Took 113ms
Downloading file [/Users/nunoguterres/Downloads/zephyr.elf]...
J-Link: Flash download: Bank 1 @ 0x18000000: 1 range affected (65536 bytes)
J-Link: Flash download: Total: 0.648s (Prepare: 0.165s, Compare: 0.150s, Erase: 0.004s, Program: 0.145s, Verify: 0.107s, Restore: 0.075s)
J-Link: Flash download: Program speed: 440 KB/s

****** Error: Verification failed @ address 0x18000000
Error while programming flash: Verify failed.

 

 

 

 

And here is the example of a connection to JLink:

 

 

 

 

JLinkExe -Device RW612 -speed 4000 -if swd
SEGGER J-Link Commander V8.10 (Compiled Sep 25 2024 14:15:06)
DLL version V8.10, compiled Sep 25 2024 14:14:53

Connecting to J-Link via USB...O.K.
Firmware: J-Link MCU-Link V1 compiled Sep 24 2024 10:57:33
Hardware version: V1.00
J-Link uptime (since boot): 0d 00h 22m 48s
S/N: 1066319194
USB speed mode: High speed (480 MBit/s)
VTref=3.300V


Type "connect" to establish a target connection, '?' for help
J-Link>connect
Device "RW612" selected.


Connecting to target via SWD
InitTarget() start
SWD selected. Executing JTAG -> SWD switching sequence.
DAP initialized successfully.
  DMAP_REG_ID: DM-AP IDCODE detected: 0x002A0000
  DHCSR: 0x05100000
InitTarget() end - Took 2.71ms
Found SW-DP with ID 0x6BA02477
DPIDR: 0x6BA02477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x84770001, ADDR: 0x00000000)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)
Feature set: Mainline
Cache: No cache
Found Cortex-M33 r0p4, Little endian.
FPUnit: 8 code (BP) slots and 0 literal slots
Security extension: implemented
Secure debug: enabled
CoreSight components:
ROMTbl[0] @ E00FF000
[0][0]: E000E000 CID B105900D PID 000BBD21 DEVARCH 47702A04 DEVTYPE 00 Cortex-M33
[0][1]: E0001000 CID B105900D PID 000BBD21 DEVARCH 47701A02 DEVTYPE 00 DWT
[0][2]: E0002000 CID B105900D PID 000BBD21 DEVARCH 47701A03 DEVTYPE 00 FPB
[0][3]: E0000000 CID B105900D PID 000BBD21 DEVARCH 47701A01 DEVTYPE 43 ITM
[0][5]: E0041000 CID B105900D PID 002BBD21 DEVARCH 47724A13 DEVTYPE 13 ETM
[0][6]: E0042000 CID B105900D PID 000BBD21 DEVARCH 47701A14 DEVTYPE 14 CSS600-CTI
Memory zones:
  Zone: "Default" Description: Default access mode
Cortex-M33 identified.

 

 

 


I've noticed this behavior has happened twice (in two boards). I really want to believe this has nothing to do with the LCD, since it would place the responsibility of this not working onto NXP/Adafruit hands and faulty design.

Has anyone experienced something like this?

 

Labels (1)
25 Replies

3,571 Views
nguterresn
Contributor II

This also happens when trying to load an image to flash:

 

 

blhost --port /dev/tty.usbmodem0010663191941 flash-image /Users/nunoguterres/mcu-expresso/RW612_Project/Debug/RW612_Project.hex erase 0x09
WARNING:spsdk.mboot.mcuboot:Note: memoryId is not required when accessing mapped external memory (149ms since start, mcuboot.py:1782)
Response status = 20106 (0x4e8a) FlexSPINOR: Command Failure.
blhost --port /dev/tty.usbmodem0010663191941 load-image /Users/nunoguterres/mcu-expresso/RW612_Project/Debug/RW612_Project.bin
Loading image  [------------------------------------]    0%ERROR:spsdk.mboot.mcuboot:RX: No Response, Timeout Error ! (5142ms since start, mcuboot.py:242)

McuBootConnectionError: MBoot: Connection issue -> No Response from Device
See debug log file: /Users/nunoguterres/Library/Logs/spsdk/2.4.0/debug.log for more info

 

0 Kudos
Reply

3,297 Views
nguterresn
Contributor II

 I also have the feeling the JLink is targeting the secure zone (0x1800_0000) whereas the blhost is targeting the non-secure zone (0x0800_0000)

J-Link>erase
No address range specified, 'Erase Chip' will be executed
'erase': Performing implicit reset & halt of MCU.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
  MSPLIM cleared
ResetTarget() end - Took 113ms
Erasing device...
J-Link: Flash download: Only internal flash banks will be erased.
To enable erasing of other flash banks like QSPI or CFI, it needs to be enabled via "exec EnableEraseAllFlashBanks"
J-Link: Flash download: Total time needed: 1.482s (Prepare: 0.199s, Compare: 0.000s, Erase: 1.176s, Program: 0.000s, Verify: 0.000s, Restore: 0.106s)
Erasing done.
J-Link>r
Reset delay: 0 ms
Reset type NORMAL: Resets core & peripherals via SYSRESETREQ & VECTRESET bit.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
  MSPLIM cleared
ResetTarget() end - Took 119ms
J-Link>mem8  0x08001000, 10
08001000 = 01 4B 0C 10 ED FC 05 18 31 14 0A 18 D9 FC 05 18 
J-Link>mem8  0x18001000, 10
18001000 = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
0 Kudos
Reply

3,295 Views
nguterresn
Contributor II

 

J-Link>erase
No address range specified, 'Erase Chip' will be executed
'erase': Performing implicit reset & halt of MCU.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
  MSPLIM cleared
ResetTarget() end - Took 113ms
Erasing device...
J-Link: Flash download: Only internal flash banks will be erased.
To enable erasing of other flash banks like QSPI or CFI, it needs to be enabled via "exec EnableEraseAllFlashBanks"
J-Link: Flash download: Total time needed: 1.482s (Prepare: 0.199s, Compare: 0.000s, Erase: 1.176s, Program: 0.000s, Verify: 0.000s, Restore: 0.106s)
Erasing done.

 

J-Link>r
Reset delay: 0 ms
Reset type NORMAL: Resets core & peripherals via SYSRESETREQ & VECTRESET bit.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
  MSPLIM cleared
ResetTarget() end - Took 119ms

 
After erasing, this is the data at 0x0800_0000:

J-Link>mem8  0x08001000, 10
08001000 = 01 4B 0C 10 ED FC 05 18 31 14 0A 18 D9 FC 05 18 

 
I really don't know what's going on. 

0 Kudos
Reply

3,225 Views
nguterresn
Contributor II

Hi,

blhost --port /dev/tty.usbmodem0010663191941 get-property 0x19 0x09
Response status = 0 (0x0) Success.
Response word 1 = 31 (0x1f)
Response word 2 = 134217728 (0x8000000)
Response word 3 = 65536 (0x10000)
Response word 4 = 256 (0x100)
Response word 5 = 4096 (0x1000)
Response word 6 = 32768 (0x8000)
External Memory Attributes = Start Address: 0x08000000, Total Size:    64.0 MiB, Page Size:     256 B, Sector Size:   4.0 kiB, Block Size:    32.0 kiB
blhost --port /dev/tty.usbmodem0010663191941 read-memory 0x08000400 100
Reading memory  [####################################]  100%
46 42 00 00 00 00 00 00 00 00 01 03 03 00 01 00
00 00 01 02 00 00 40 c7 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 01 04 07 00 00 00 00 00 00 00 00 00 00 00
00 04 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00
Response status = 0 (0x0) Success.
Response word 1 = 100 (0x64)
Read 100 of 100 bytes.


FCB (@x400) looks odd!

blhost --port /dev/tty.usbmodem0010663191941 get-property 0x11              
Response status = 0 (0x0) Success.
Response word 1 = 1520786085 (0x5aa55aa5)
Response word 2 = 3 (0x3)
Security State = UNSECURE
blhost --port /dev/tty.usbmodem0010663191941 get-property 0x0a              
Response status = 0 (0x0) Success.
Response word 1 = 1 (0x1)
Verify Writes = ON


I'm not able to write using blhost, but with JLink:

blhost --port /dev/tty.usbmodem0010663191941 fill-memory 0x08001000 10 0x01 
Response status = 10203 (0x27db) Memory Cumulative Write.
blhost --port /dev/tty.usbmodem0010663191941 write-memory 0x08000000 {{aabbccdd}}
Writing memory  [####################################]  100%
Response status = 10203 (0x27db) Memory Cumulative Write.


 

J-Link>Write1 0x08001000, 0x01
Writing 01 -> 08001000
J-Link>mem8  0x08001000, 10
08001000 = 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 



> Do you recall what was the last application you were able to flash?
 
It was probably the zephyr sample Blinky for this board. But can't be 100% sure.


 

0 Kudos
Reply

3,230 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

Are you able to write on flash?

Do you recall what was the last application you were able to flash?

Regards,

Daniel.

0 Kudos
Reply