FRDM- MCXW71

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,799件の閲覧回数
Shreyas_Bhat
Contributor II

Hi i have bought FRDM MCxW71 for home automation project and am comfortable with S32DS is there a way to get drivers and build the project using s32DS
thank you 

ラベル(2)
0 件の賞賛
返信
1 解決策
1,791件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @Shreyas_Bhat ,

Thanks for your post.

You can download SDK from here: Select Board | MCUXpresso SDK Builder


Please refer to the figure below. Currently, we only support the following three IDEs(MCUXPresso, MCUXpresso for VSCode, IAR) for FRDM-MCXW71, which do not include S32DS. S32DS is designed for our automotive production line.


Thank you for your understanding.

Celeste_Liu_0-1747974163952.png

And kindly note that questions related to MCXW should be raised in the following forum to obtain better support.

Wireless MCU - NXP Community

 

BRs,

Celeste

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

元の投稿で解決策を見る

3 返答(返信)
1,792件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @Shreyas_Bhat ,

Thanks for your post.

You can download SDK from here: Select Board | MCUXpresso SDK Builder


Please refer to the figure below. Currently, we only support the following three IDEs(MCUXPresso, MCUXpresso for VSCode, IAR) for FRDM-MCXW71, which do not include S32DS. S32DS is designed for our automotive production line.


Thank you for your understanding.

Celeste_Liu_0-1747974163952.png

And kindly note that questions related to MCXW should be raised in the following forum to obtain better support.

Wireless MCU - NXP Community

 

BRs,

Celeste

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

1,771件の閲覧回数
Shreyas_Bhat
Contributor II
Is there a pin gui based configuration in mcxpresso ide
0 件の賞賛
返信
1,767件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Yes, we have MCUXpresso config tools. 

MCUXpresso Config Tools | Software Development for NXP Microcontrollers (MCUs) | NXP Semiconductors

After you installed the MCUXpresso IDE, you can find it here.

Celeste_Liu_0-1747978702683.png

 

BRs,

Celeste