FRDM-MCXN947 - LPUART With PLL0 CLK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-MCXN947 - LPUART With PLL0 CLK

Jump to solution
1,481 Views
John_Adams
Contributor I

Hello,
I am trying to use LPUART on FRO_HF (48MHz) with baudrate 320400, but MCUs with interrupt are not able to receive all characters, so there are frequent communication failures. How is it possible to connect to LPUART a clock from PLL0 running at 150MHz? Is it necessary to configure PLL0 somehow?

0 Kudos
Reply
1 Solution
1,458 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @John_Adams,

I believe this is a duplicated community post from the one seen here: UART Setup on FRDM-MCXN947 - NXP Community

In order to prevent double efforts, I will continue supporting you on the aforementioned post.

Have a nice day.

BR,
Edwin. 

View solution in original post

0 Kudos
Reply
1 Reply
1,459 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @John_Adams,

I believe this is a duplicated community post from the one seen here: UART Setup on FRDM-MCXN947 - NXP Community

In order to prevent double efforts, I will continue supporting you on the aforementioned post.

Have a nice day.

BR,
Edwin. 

0 Kudos
Reply