I am trying to use a Segger J-Link JTAG with the FRDM-MCXA156, and no matter the jumper configuration I am unable to get the Segger tools to connect to the processor. Lotest Segger tools installed, J-Link firmware updated to latest version.
Ultimately I plan to use IAR tools with the Segger J-Link, but for now, I am just trying to get the J-Link to work. Any suggestions are welcome.
When I try to connect to the processor using J-Link Commander V9.36, it goes through the motions, but fails with :
****** Error: J-Link script file function InitTarget() returned with error code -1
Error occurred: Could not connect to the target device.
For troubleshooting steps visit: https://kb.segger.com/J-Link_Troubleshooting
J-Link>