Hello,
I read AN14558 (Low Power Implementation on MCX A153 MCU Series) and used the program included in this application note. I obtained almost identical results, which match those shown in https://www.youtube.com/watch?v=Rj9QANRU3rA.
In sleep mode with slow wake-up (options B and 3 in the terminal), the current is 0.85 mA.
In the MCXAP64M96FS3 datasheet, the table 14 in section 3.2.6.1 states that IDD_SLEEP_MD should be 0.34 mA. That is less than half of the value specified in AN14558.
What else needs to be changed in the program to get the current closer to 0.34 mA?
I’ve studied the application note and the source code; in my opinion, everything is set for minimum current consumption.
Thank you, Petr