Does eIQ NPU on MCXN947 support transformer based model?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does eIQ NPU on MCXN947 support transformer based model?

293 次查看
TomC818
Contributor III

Hello,
As mentioned in the title, can the NPU in the mcu support transformer based model? From the official website, it was claimed that the NPU can support transformer models.

TomC818_0-1755162965843.png
Assuming with compression, quantization and external RAM through flexspi, a small transformer based model can be fitted on board. Can the NPU actually be used to accelerate the inference? 

An example would be GitHub - maxbbraun/llama4micro: A "large" language model running on a microcontroller
Instead of running on the CPU, can the model be ran on the NPU? 
How can such a use case be adapted to MCXN?

 

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

242 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @TomC818 

Full “LLM on NPU” isn’t a supported path yet on MCX.

LLMs rely on dynamic sequences, KV caches, etc.—many are outside the current eIQ Neutron TFLite op set.

BR

Harry

0 项奖励
回复