Does MCXC44x support 5V SLCD?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MCXC44x support 5V SLCD?

Jump to solution
1,719 Views
jimmyli
Contributor V

Hi,

    Our customer is evaluating mcxc44x to drive slcd directly, but the slcd is power by 5Vdc.

    Can MCXC44x support it?

 

    Thanks very much.

Labels (1)
0 Kudos
Reply
1 Solution
1,705 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @jimmyli ,

Thanks for your post.  The MCXC44x does not support 5V SLCD. According to Data Sheet, whether configured as an internal or external power, the maximum voltage should not exceed VDD, which is within the range of 1.71 to 3.6V. 

Wish it helps.

 

----------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
----------------------------------------------------------------------------------------

Best Regards,

Celeste

View solution in original post

0 Kudos
Reply
2 Replies
1,706 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @jimmyli ,

Thanks for your post.  The MCXC44x does not support 5V SLCD. According to Data Sheet, whether configured as an internal or external power, the maximum voltage should not exceed VDD, which is within the range of 1.71 to 3.6V. 

Wish it helps.

 

----------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
----------------------------------------------------------------------------------------

Best Regards,

Celeste

0 Kudos
Reply
1,700 Views
jimmyli
Contributor V

Hi Celeste,

       Got it.

       Thanks.

0 Kudos
Reply