Difference between MCUXpresso and Datasheet on OPAMPs for MCX A365

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between MCUXpresso and Datasheet on OPAMPs for MCX A365

Jump to solution
1,071 Views
nxpenthusiast
Contributor I

I am doing a project that needs 3 opamps on one MCU and selected the MXC A365 in the LQFP64 pin package. On the datasheet, it shows there should be 3 opamps. When I started doing peripheral assignment in MCUXpresso, it only lists OPAMP0 and OPAMP 2 as choices. There is no 3rd opamp choice. Is there a different way to enable the 3rd opamp or is the datasheet wrong? 

I've attached screen shots of the datasheet and what MCUXpresso shows. 

Labels (3)
0 Kudos
Reply
1 Solution
886 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @nxpenthusiast ,

Thanks for your patience. I got the confirmation from the internal.

For LQFP64 package,

  • MCXA34x/35x devices have 3 OPAMPs
  • MCXA36x devices have 2 OPAMPs

Please refer to latest datasheet:

Mixed-signal Arm Cortex-M33 MCU with 180/240 MHz, up to 1024 KB Flash

 

Celeste_Liu_0-1776825810314.png

 

Sorry for the inconvenience caused.

BR

Celeste

View solution in original post

3 Replies
1,034 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @nxpenthusiast ,

Thank you for bringing this issue to our attention. I’ve checked it, and there is indeed an inconsistency as you described. I’ll need to verify this internally, and I’ll keep you informed once I receive a confirmed answer.
Have a nice day.
BR
Celeste
0 Kudos
Reply
1,019 Views
nxpenthusiast
Contributor I

Thank you! I appreciate the expedient response. 

0 Kudos
Reply
888 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @nxpenthusiast ,

Thanks for your patience. I got the confirmation from the internal.

For LQFP64 package,

  • MCXA34x/35x devices have 3 OPAMPs
  • MCXA36x devices have 2 OPAMPs

Please refer to latest datasheet:

Mixed-signal Arm Cortex-M33 MCU with 180/240 MHz, up to 1024 KB Flash

 

Celeste_Liu_0-1776825810314.png

 

Sorry for the inconvenience caused.

BR

Celeste