Debug In MCUExpressoIDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug In MCUExpressoIDE

1,204件の閲覧回数
PoojaAgri
Contributor I

Hello, 

I am trying to flash my device using the MCUXpressoIDE. I am using this Debug icon in the QuickStart panel

#MKE14Zxxxxxx7

PoojaAgri_0-1718690673481.pngPoojaAgri_0-1718690673481.png

It is able to discover probe but in console it shows probe not found and when I select the probe in the screen, it quits and does not start the debug session. If anybody faced the similar problem and resolved it, please help me out here.

PoojaAgri_1-1718690830161.pngPoojaAgri_1-1718690830161.png

PoojaAgri_2-1718690951832.pngPoojaAgri_2-1718690951832.png

 

 

ラベル(1)
0 件の賞賛
返信
1 返信

1,178件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @PoojaAgri 

Based on this phenomenon, it indicates that your IDE has recognized the jlink, so make sure that the J-Link probe is properly connected to your device.

If possible, try using a different debug probe to see if the problem persists.

Hope this will help you.

BR

Hang

0 件の賞賛
返信